NXOpen.UF.Assem.IsetArrayData Structure¶
NXOpen.UF.Assem.IsetArrayData is an alias for NXOpen.UF.AssemIsetArrayData_Struct
-
class
NXOpen.UF.
AssemIsetArrayData_Struct
¶ Bases:
object
Refer to UF_ASSEM_iset_array_data_s for documentation.
Fields
NXOpen.UF.AssemIsetArrayData_Struct.FeatureIset |
The tag of the feature iset that the array is based upon. |
NXOpen.UF.AssemIsetArrayData_Struct.TemplateComponent |
The tag of the template component for this array. |
NXOpen.UF.AssemIsetArrayData_Struct.Dimensions |
An array of integers which indicates the size of the array. |
NXOpen.UF.AssemIsetArrayData_Struct.ArrayName |
The name of the array object. |