NXOpen.UF.Assem.GetRefSetInst¶
-
Assem.
GetRefSetInst
()¶ Refer to UF_ASSEM_get_ref_set_inst for documentation.
Signature:
GetRefSetInst(objectArg, number)
Parameters: - objectArg (Tag) – Object Identifier (object can be an occurrence)
- number (int) – The number of the reference set to which the object belongs (e.g. 1 is the first reference set it belongs to, 2 is the second reference set, etc.).
Returns: Object Identifier of the numbered reference setthat contains the object. NULL_TAG is returned when theobject does not belong to any reference sets or if ithas less than number links.
Return type: License requirements: None