NXOpen.UF.Assem.EvalInstanceIntent¶
-
Assem.
EvalInstanceIntent
()¶ Refer to UF_ASSEM_eval_instance_intent for documentation.
Signature:
EvalInstanceIntent(instance, applyResult)
Parameters: - instance (Tag) – Object identifier of the instance. Note that the instance tag is not currently modified; but it may be modified in the future (hence, its designation as an I/O parameter).
- applyResult (bool) – Apply result flag.
Returns: A Tuple
Return type: A tuple consisting of (instance,instanceStatus)
instance(Tag): Modified value of instance
instanceStatus(
`NXOpen.UF.Assem.InstanceStatus
Refer to UF_ASSEM_instance_status_s for documentation.`): Status of the instance.License requirements: ASSEMBLIES MODULE