NXOpen.UF.Assem.CopyExplosion¶
-
Assem.
CopyExplosion
()¶ Refer to UF_ASSEM_copy_explosion for documentation.
Signature:
CopyExplosion(sourceExplosion, sourceComponent, destinationExplosion, destinationComponent)
Parameters: - sourceExplosion (Tag) – The tag of the explosion from which to copy transforms.
- sourceComponent (Tag) – Either NULL_TAG, in which case the whole explosion is copied, or a component (part occurrence) tag indicating the portion of the explosion to be copied.
- destinationExplosion (Tag) – The tag of the explosion which the source explosion should be copied into.
- destinationComponent (Tag) – Either NULL_TAG, in which case the whole explosion is over-written, or a component (part occurrence) tag indicating a portion of the explosion to be over-written (in either case, the tag must represent the same componenrt part as the source_component argument).
License requirements: ASSEMBLIES MODULE