WorkpieceBuilderWorkPieceType Enumeration

NXOpen.Tooling.WorkpieceBuilder.WorkPieceType is an alias for NXOpen.Tooling.WorkpieceBuilderWorkPieceType

class NXOpen.Tooling.WorkpieceBuilderWorkPieceType

Bases: object

the unit type includes the work piece create method

Enum Members

Enum Member Enum Member Description
UserDefinedBlock
The method defines the block by user
CavityCore
The method adds the standards of cavity and core
CavityOnly
The method adds the standards of cavity
CoreOnly
The method adds the standards of cavity
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.