WorkpieceBuilderTypes Enumeration

NXOpen.Tooling.WorkpieceBuilder.Types is an alias for NXOpen.Tooling.WorkpieceBuilderTypes

class NXOpen.Tooling.WorkpieceBuilderTypes

Bases: object

the unit type includes product and combined work piece type

Enum Members

Enum Member Enum Member Description
ProductWorkPiece
The old assembly of Mold wizard
CombinedWorkPiece
The new assembly of Mold wizard
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.