ValidCheckBuilderSelMode Enumeration

NXOpen.Tooling.ValidCheckBuilder.SelMode is an alias for NXOpen.Tooling.ValidCheckBuilderSelMode

class NXOpen.Tooling.ValidCheckBuilderSelMode

Bases: object

the selection type, including component and solid body

Enum Members

Enum Member Enum Member Description
Component
Selection type will be set to component
Body
Selection type will be set to body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.