ValidCheckBuilderCheckingType Enumeration

NXOpen.Tooling.ValidCheckBuilder.CheckingType is an alias for NXOpen.Tooling.ValidCheckBuilderCheckingType

class NXOpen.Tooling.ValidCheckBuilderCheckingType

Bases: object

the checking type, including true body, false body or both

Enum Members

Enum Member Enum Member Description
TrueBody
True body will be used to do checking
FalseBody
False body will be used to do checking
Both
Both types of body will be used to do checking
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.