ValidCheckBuilderAnalysisMode Enumeration

NXOpen.Tooling.ValidCheckBuilder.AnalysisMode is an alias for NXOpen.Tooling.ValidCheckBuilderAnalysisMode

class NXOpen.Tooling.ValidCheckBuilderAnalysisMode

Bases: object

the analysis mode, including solid-based mode and facet-based mode

Enum Members

Enum Member Enum Member Description
SolidBased
Solid body will be used to do checking
FacetBased
Facet body will be used to do checking
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.