UniversalUnformBuilder Class¶
-
class
NXOpen.Tooling.
UniversalUnformBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Tooling.UniversalUnformBuilder
builder.To create a new instance of this class, use
NXOpen.Features.ToolingCollection.CreateUniversalUnformBuilder()
Default values.
Property Value BendType StraightBend DefineNeutralFactor.BendDevelopedLength 0 DefineNeutralFactor.NeutralFactor 0.40 DefineNeutralFactor.NeutralFactorFormula General DefineNeutralFactor.PartMaterial 08 UnformNeutralFactor (deprecated) 0.4 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
BendFaces | Returns the bend faces |
BendType | Returns or sets the bend type |
BlendFaces | Returns the blend faces |
DefineNeutralFactor | Returns the define neutral factor builder which contains new neutral factor, part material and bend developed length |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceFaceEdge | Returns the reference face edge |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UnformNeutralFactor | Returns or sets the operation of neutral factor for univeral unform. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
UniversalUnformBuilderBendTypes Enumeration | The types of bend |
Property Detail¶
BendFaces¶
-
UniversalUnformBuilder.
BendFaces
¶ Returns the bend faces
-------------------------------------
Getter Method
Signature
BendFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
BendType¶
-
UniversalUnformBuilder.
BendType
¶ Returns or sets the bend type
-------------------------------------
Getter Method
Signature
BendType()
Returns: Return type: NXOpen.Tooling.UniversalUnformBuilderBendTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendType(bendType)
Parameters: bendType ( NXOpen.Tooling.UniversalUnformBuilderBendTypes
) –New in version NX8.5.0.
License requirements: None.
BlendFaces¶
-
UniversalUnformBuilder.
BlendFaces
¶ Returns the blend faces
-------------------------------------
Getter Method
Signature
BlendFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
DefineNeutralFactor¶
-
UniversalUnformBuilder.
DefineNeutralFactor
¶ Returns the define neutral factor builder which contains new neutral factor, part material and bend developed length
-------------------------------------
Getter Method
Signature
DefineNeutralFactor()
Returns: Return type: NXOpen.Tooling.DefineNeutralFactorBuilder
New in version NX10.0.0.
License requirements: None.
ReferenceFaceEdge¶
-
UniversalUnformBuilder.
ReferenceFaceEdge
¶ Returns the reference face edge
-------------------------------------
Getter Method
Signature
ReferenceFaceEdge()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
UnformNeutralFactor¶
-
UniversalUnformBuilder.
UnformNeutralFactor
¶ Returns or sets the operation of neutral factor for univeral unform.
-------------------------------------
Getter Method
Signature
UnformNeutralFactor()
Returns: Return type: float New in version NX8.5.0.
Deprecated since version NX10.0.0: Use
Tooling.DefineNeutralFactorBuilder.NeutralFactor()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
UnformNeutralFactor(kFactor)
Parameters: kFactor (float) – New in version NX8.5.0.
Deprecated since version NX10.0.0: Use
Tooling.DefineNeutralFactorBuilder.NeutralFactor()
instead.License requirements: None.
Method Detail¶
Validate¶
-
UniversalUnformBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.