UndersizeBuilder Class¶
-
class
NXOpen.Tooling.
UndersizeBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.UndersizeBuilder
To create a new instance of this class, use
NXOpen.Tooling.UndersizeCollection.CreateUndersizeBuilder()
Default values.
Property Value Angle.Value 90 (millimeters part), 90 (inches part) OrbitSize.Value 0.05 (millimeters part), 0.002 (inches part) OrbitType Circular SparkGap.Value 0.05 (millimeters part), 0.002 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle which is between two distribution electrodes |
ElectrodeBodies | Returns the electrode body to do undersize |
OrbitPointList | Returns the points to be used as copy positions to undersize electrode |
OrbitSize | Returns the orbit size which determines the radius of the distribution circle |
OrbitType | Returns or sets the orbit type |
PointSpecify | Returns or sets the reference point which is the center of the distribution circle |
SelectElectrodeBlock | Returns the body will be used as electrode body to do undersize |
SelectPoints | Returns the points will be used as copy positions to undersize electrode |
SparkGap | Returns the spark gap which is the gap between the electrode head and the work piece |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
UndersizeBuilderOrbit Enumeration | Represents the orbit type |
Property Detail¶
Angle¶
-
UndersizeBuilder.
Angle
¶ Returns the angle which is between two distribution electrodes
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
ElectrodeBodies¶
-
UndersizeBuilder.
ElectrodeBodies
¶ Returns the electrode body to do undersize
-------------------------------------
Getter Method
Signature
ElectrodeBodies()
Returns: Return type: NXOpen.SelectBodyList
New in version NX10.0.0.
License requirements: None.
OrbitPointList¶
-
UndersizeBuilder.
OrbitPointList
¶ Returns the points to be used as copy positions to undersize electrode
-------------------------------------
Getter Method
Signature
OrbitPointList()
Returns: Return type: NXOpen.SelectPointList
New in version NX10.0.0.
License requirements: None.
OrbitSize¶
-
UndersizeBuilder.
OrbitSize
¶ Returns the orbit size which determines the radius of the distribution circle
-------------------------------------
Getter Method
Signature
OrbitSize()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
OrbitType¶
-
UndersizeBuilder.
OrbitType
¶ Returns or sets the orbit type
-------------------------------------
Getter Method
Signature
OrbitType()
Returns: Return type: NXOpen.Tooling.UndersizeBuilderOrbit
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrbitType(orbitType)
Parameters: orbitType ( NXOpen.Tooling.UndersizeBuilderOrbit
) –New in version NX6.0.0.
License requirements: None.
PointSpecify¶
-
UndersizeBuilder.
PointSpecify
¶ Returns or sets the reference point which is the center of the distribution circle
-------------------------------------
Getter Method
Signature
PointSpecify()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSpecify(pointSpecify)
Parameters: pointSpecify ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
SelectElectrodeBlock¶
-
UndersizeBuilder.
SelectElectrodeBlock
¶ Returns the body will be used as electrode body to do undersize
-------------------------------------
Getter Method
Signature
SelectElectrodeBlock()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Tooling.UndersizeBuilder.ElectrodeBodies()
instead.License requirements: None.
SelectPoints¶
-
UndersizeBuilder.
SelectPoints
¶ Returns the points will be used as copy positions to undersize electrode
-------------------------------------
Getter Method
Signature
SelectPoints()
Returns: Return type: NXOpen.SelectPointList
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Tooling.UndersizeBuilder.OrbitPointList()
instead.License requirements: None.
SparkGap¶
-
UndersizeBuilder.
SparkGap
¶ Returns the spark gap which is the gap between the electrode head and the work piece
-------------------------------------
Getter Method
Signature
SparkGap()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
UndersizeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.