TrimMoldComponentsBuilderTargetScope Enumeration

NXOpen.Tooling.TrimMoldComponentsBuilder.TargetScope is an alias for NXOpen.Tooling.TrimMoldComponentsBuilderTargetScope

class NXOpen.Tooling.TrimMoldComponentsBuilderTargetScope

Bases: object

the target bodies selection scope

Enum Members

Enum Member Enum Member Description
Product
Select target bodies in product node part
Any
Select target bodies in any part of the entire assembly
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.