ToolingClonemethod Enumeration

class NXOpen.Tooling.ToolingClonemethod

Bases: object

Clone method Enum Members

Enum Member Enum Member Description
UseLogFile
Use clone log file method
Rename
Use part rename method
SaveAs
Use part save as method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.