ToolingApplication Enumeration

class NXOpen.Tooling.ToolingApplication

Bases: object

Wizard type, some of them should be same as in mpdwshare_uf_mold.

h Enum Members

Enum Member Enum Member Description
ReuseLibrary
Reuse Library
MoldWizard
MoldWizard
PdieWizard
Progressive Die Wizard
StampingDie
Stamping Die
ElectrodeWizard
Electrode Wizard
EdieWizard
Engineering Die Wizard
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.