SubInsertBuilderTypes Enumeration

NXOpen.Tooling.SubInsertBuilder.Types is an alias for NXOpen.Tooling.SubInsertBuilderTypes

class NXOpen.Tooling.SubInsertBuilderTypes

Bases: object

Represents the type of parent part

Enum Members

Enum Member Enum Member Description
ParentOfSolidOwningPart
The parent part is the parent of solid owning part
ProdPart
The parent part is Prod part
SolidOwningPart
The parent part is the owning part of solid
CurrentWorkPart
The parent part is current work part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.