StockSizeBuilderTypes Enumeration

NXOpen.Tooling.StockSizeBuilder.Types is an alias for NXOpen.Tooling.StockSizeBuilderTypes

class NXOpen.Tooling.StockSizeBuilderTypes

Bases: object

Represents the shape of stock size.

Enum Members

Enum Member Enum Member Description
Block
The shape is a block
Cylinder
The shape is a cylinder
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.