StockSizeBuilderRefCsysType Enumeration

NXOpen.Tooling.StockSizeBuilder.RefCsysType is an alias for NXOpen.Tooling.StockSizeBuilderRefCsysType

class NXOpen.Tooling.StockSizeBuilderRefCsysType

Bases: object

Represents the reference CSYS type.

Enum Members

Enum Member Enum Member Description
Wcs
reference WCS
AbsoluteDisplayedPart
reference ABS in displayed part
SelectedCSYS
reference the selected csys
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.