StandardPartPositionBuilder Class¶
-
class
NXOpen.Tooling.
StandardPartPositionBuilder
¶ Bases:
NXOpen.Builder
Represents a StandardPartPositionBuilder to add or edit a standard part in the selected plane with specified position.
To create a new instance of this class, use
NXOpen.Tooling.StandardPartPositionCollection.CreateStandardPartPositionBuilder()
Default values.
Property Value AssociativePosition 1 DxIncrement 1.0 DyIncrement 1.0 OffsetPositionDx.Value 0.0 (millimeters part), 0.0 (inches part) OffsetPositionDy.Value 0.0 (millimeters part), 0.0 (inches part) New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AssociativePosition | Returns or sets the associative status between standardpart and the offset point. |
DxIncrement | Returns or sets the increment in X direction when a standard part is dragged. |
DyIncrement | Returns or sets the increment in Y direction when a standard part is dragged. |
OffsetPositionDx | Returns the dimension in X direction from reference point to offset point. |
OffsetPositionDy | Returns the dimension in Y direction from reference point to offset point. |
ReferencePosition | Returns or sets the reference point position. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PlaneView | Sets the view to the selected face plane or X-Y plane of WCS. |
SetFaceCenter | Sets the reference point to the selected face center. |
SetOffsetPosition | The offset point position. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssociativePosition¶
-
StandardPartPositionBuilder.
AssociativePosition
¶ Returns or sets the associative status between standardpart and the offset point.
-------------------------------------
Getter Method
Signature
AssociativePosition()
Returns: Return type: bool New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
AssociativePosition(associativePosition)
Parameters: associativePosition (bool) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DxIncrement¶
-
StandardPartPositionBuilder.
DxIncrement
¶ Returns or sets the increment in X direction when a standard part is dragged.
-------------------------------------
Getter Method
Signature
DxIncrement()
Returns: Return type: float New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
DxIncrement(dxIncrement)
Parameters: dxIncrement (float) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DyIncrement¶
-
StandardPartPositionBuilder.
DyIncrement
¶ Returns or sets the increment in Y direction when a standard part is dragged.
-------------------------------------
Getter Method
Signature
DyIncrement()
Returns: Return type: float New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
DyIncrement(dyIncrement)
Parameters: dyIncrement (float) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositionDx¶
-
StandardPartPositionBuilder.
OffsetPositionDx
¶ Returns the dimension in X direction from reference point to offset point.
-------------------------------------
Getter Method
Signature
OffsetPositionDx()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositionDy¶
-
StandardPartPositionBuilder.
OffsetPositionDy
¶ Returns the dimension in Y direction from reference point to offset point.
-------------------------------------
Getter Method
Signature
OffsetPositionDy()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ReferencePosition¶
-
StandardPartPositionBuilder.
ReferencePosition
¶ Returns or sets the reference point position.
-------------------------------------
Getter Method
Signature
ReferencePosition()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
ReferencePosition(refPos)
Parameters: refPos ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
PlaneView¶
-
StandardPartPositionBuilder.
PlaneView
¶ Sets the view to the selected face plane or X-Y plane of WCS.
Signature
PlaneView()
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetFaceCenter¶
-
StandardPartPositionBuilder.
SetFaceCenter
¶ Sets the reference point to the selected face center.
Signature
SetFaceCenter()
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetOffsetPosition¶
-
StandardPartPositionBuilder.
SetOffsetPosition
¶ The offset point position.
Signature
SetOffsetPosition(position)
Parameters: position ( NXOpen.Point3d
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
StandardPartPositionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.