SpreadsheetDataKeywordType Enumeration¶
NXOpen.Tooling.SpreadsheetData.KeywordType is an alias for NXOpen.Tooling.SpreadsheetDataKeywordType
-
class
NXOpen.Tooling.
SpreadsheetDataKeywordType
¶ Bases:
object
Represents the different attribute or expression section in spreadsheet
Enum Members
Enum Member Enum Member Description ObjectAttribute Object attribute defined in spreadsheetPartAttribute Part attribute defined in spreadsheetExpression Expression defined in spreadsheet-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-