SplitSolidBuilderToolObjectOption Enumeration

NXOpen.Tooling.SplitSolidBuilder.ToolObjectOption is an alias for NXOpen.Tooling.SplitSolidBuilderToolObjectOption

class NXOpen.Tooling.SplitSolidBuilderToolObjectOption

Bases: object

the split tool selection type: Existing Object, New Plane.

Enum Members

Enum Member Enum Member Description
ExistingObject
Existing Object option
NewPlane
New Plane option
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.