SpecifyBaffleBuilder Class¶
-
class
NXOpen.Tooling.
SpecifyBaffleBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to be used to create specify baffle.
To create a new instance of this class, use
NXOpen.Tooling.SpecifyBaffleCollection.CreateBuilder()
Default values.
Property Value AttributeType BodyAsChannel Layer 1 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AttributeType | Returns or sets the type of attributes conversion type values. |
ChannelColor | Returns or sets the selected channel body color. |
ChannelType | Returns or sets the type to specify the Cooling fittings types: oil, air or water. |
Channels | Returns the channel or body to assign new attributes. |
Layer | Returns or sets the layer value for the selected channels. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetColorModified | Sets the color value modified or not. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpecifyBaffleBuilderAttributeTypes Enumeration | Types to specify how to assign attributes to the selected body. |
Property Detail¶
AttributeType¶
-
SpecifyBaffleBuilder.
AttributeType
¶ Returns or sets the type of attributes conversion type values.
-------------------------------------
Getter Method
Signature
AttributeType()
Returns: Return type: NXOpen.Tooling.SpecifyBaffleBuilderAttributeTypes
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
-------------------------------------
Setter Method
Signature
AttributeType(attrType)
Parameters: attrType ( NXOpen.Tooling.SpecifyBaffleBuilderAttributeTypes
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
ChannelColor¶
-
SpecifyBaffleBuilder.
ChannelColor
¶ Returns or sets the selected channel body color.
-------------------------------------
Getter Method
Signature
ChannelColor()
Returns: Return type: Id New in version NX8.0.1.
License requirements: ug_mold_design (“UG MOLD”)
-------------------------------------
Setter Method
Signature
ChannelColor(channelColor)
Parameters: channelColor (Id) – New in version NX8.0.1.
License requirements: ug_mold_design (“UG MOLD”)
ChannelType¶
-
SpecifyBaffleBuilder.
ChannelType
¶ Returns or sets the type to specify the Cooling fittings types: oil, air or water.
-------------------------------------
Getter Method
Signature
ChannelType()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChannelType(channelType)
Parameters: channelType (str) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Channels¶
-
SpecifyBaffleBuilder.
Channels
¶ Returns the channel or body to assign new attributes.
-------------------------------------
Getter Method
Signature
Channels()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Layer¶
-
SpecifyBaffleBuilder.
Layer
¶ Returns or sets the layer value for the selected channels.
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Method Detail¶
SetColorModified¶
-
SpecifyBaffleBuilder.
SetColorModified
¶ Sets the color value modified or not.
Signature
SetColorModified(modified)
Parameters: modified (bool) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Validate¶
-
SpecifyBaffleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.