SpecialPiercingInsertBuilderNormalDieShoeSlugType Enumeration¶
NXOpen.Tooling.SpecialPiercingInsertBuilder.NormalDieShoeSlugType is an alias for NXOpen.Tooling.SpecialPiercingInsertBuilderNormalDieShoeSlugType
-
class
NXOpen.Tooling.
SpecialPiercingInsertBuilderNormalDieShoeSlugType
¶ Bases:
object
Specifies the type of die shoe slug.
Enum Members
Enum Member Enum Member Description Fillet Die shoe slug type is filletRectangle Die shoe slug type is rectangleCircle Die shoe slug type is circleMickey Die shoe slug type is mickeyClearance Die shoe slug type is clearanceSlotVer Die shoe slug type is slot verticalSlotHor Die shoe slug type is slot horizontalNotSet Die shoe slug type is none-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-