SpecialPiercingInsertBuilderNormalBottomBackingPlateSlugType Enumeration¶
NXOpen.Tooling.SpecialPiercingInsertBuilder.NormalBottomBackingPlateSlugType is an alias for NXOpen.Tooling.SpecialPiercingInsertBuilderNormalBottomBackingPlateSlugType
-
class
NXOpen.Tooling.
SpecialPiercingInsertBuilderNormalBottomBackingPlateSlugType
¶ Bases:
object
Specifies the type of bottom plate slug.
Enum Members
Enum Member Enum Member Description Fillet Bottom backing plate slug type is filletRectangle Bottom backing plate slug type is rectangleCircle Bottom backing plate slug type is circleMickey Bottom backing plate slug type is mickeyClearance Bottom backing plate slug type is clearanceSlotVer Bottom backing plate slug type is slot verticalSlotHor Bottom backing plate slug type is slot horizontalNotSet Bottom backing plate slug type is none-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-