SolidPatchBuilderSolidPatchType Enumeration

NXOpen.Tooling.SolidPatchBuilder.SolidPatchType is an alias for NXOpen.Tooling.SolidPatchBuilderSolidPatchType

class NXOpen.Tooling.SolidPatchBuilderSolidPatchType

Bases: object

Settings of the solid patch creation types.

Enum Members

Enum Member Enum Member Description
SolidPatch
Solid patch type indicates to create solid patch
LinkBody
Link body type indicates to create link body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.