SmartScrewUpdateBuilder Class¶
-
class
NXOpen.Tooling.
SmartScrewUpdateBuilder
¶ Bases:
NXOpen.Builder
Smart Screw Update of MW, PDW and EDW.
No entity is returned. To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateSmartScrewUpdateBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ParentNode | Returns or sets the parent node |
Tag | Returns the Tag for this object. |
Type | Returns or sets the operation type of Tooling Part Family Part Tool. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SmartScrewUpdateBuilderParentOption Enumeration | Specify the parent node. |
SmartScrewUpdateBuilderTypes Enumeration | Specify the operation type. |
Property Detail¶
ParentNode¶
-
SmartScrewUpdateBuilder.
ParentNode
¶ Returns or sets the parent node
-------------------------------------
Getter Method
Signature
ParentNode()
Returns: Return type: NXOpen.Tooling.SmartScrewUpdateBuilderParentOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentNode(parentNode)
Parameters: parentNode ( NXOpen.Tooling.SmartScrewUpdateBuilderParentOption
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Type¶
-
SmartScrewUpdateBuilder.
Type
¶ Returns or sets the operation type of Tooling Part Family Part Tool.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.SmartScrewUpdateBuilderTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.SmartScrewUpdateBuilderTypes
) –New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
SmartScrewUpdateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.