SIZERImportBuilderPositionMode Enumeration

NXOpen.Tooling.SIZERImportBuilder.PositionMode is an alias for NXOpen.Tooling.SIZERImportBuilderPositionMode

class NXOpen.Tooling.SIZERImportBuilderPositionMode

Bases: object

Represents the position mode.

Enum Members

Enum Member Enum Member Description
InferredOnly
Inferred Only
AbsoluteOrigin
Absolute Origin
SelectOrigin
Select Origin
ByConstraints
By Constraints
Move
Move
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.