SIZERExportBuilder Class¶
-
class
NXOpen.Tooling.
SIZERExportBuilder
¶ Bases:
NXOpen.Builder
Exports input parameters for motor selection to SIZER drive design to support the sizing, configuration, and selection of drive components.
To create a new instance of this class, use
NXOpen.Tooling.SIZERCollection.CreateExportBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
OutputFile | Returns or sets the output *. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMcdMechanicalData | Gets all groups of mechanical data in MCD mode. |
GetMechanicalData | Gets all groups of mechanical data in Motion mode. |
GetObject | Returns the object currently being edited by this builder. |
GetRunMode | Gets the run mode. |
ProcessMcdSimulationData | Processes the simulation data in MCD mode. |
SetMcdMechanicalData | Sets all groups of mechanical data in MCD mode. |
SetMechanicalData | Sets all groups of mechanical data in Motion mode. |
SetRunMode | Sets the run mode. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SIZERExportBuilderRunMode Enumeration | Represents the run mode. |
Structs¶
SIZERExportBuilderMCDMechanicalData_Struct Struct | Defines the mechanical data in MCD mode. |
SIZERExportBuilderMechanicalData_Struct Struct | Defines the mechanical data in Motion mode. |
Property Detail¶
OutputFile¶
-
SIZERExportBuilder.
OutputFile
¶ Returns or sets the output *.
mdix file, which is exported to SIZER.
-------------------------------------
Getter Method
Signature
OutputFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile(outputFile)
Parameters: outputFile (str) – New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”) OR nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetMcdMechanicalData¶
-
SIZERExportBuilder.
GetMcdMechanicalData
¶ Gets all groups of mechanical data in MCD mode.
Signature
GetMcdMechanicalData()
Returns: Array of mechanical data Return type: list of NXOpen.Tooling.SIZERExportBuilderMCDMechanicalData_Struct
New in version NX9.0.0.
License requirements: None.
GetMechanicalData¶
-
SIZERExportBuilder.
GetMechanicalData
¶ Gets all groups of mechanical data in Motion mode.
Signature
GetMechanicalData()
Returns: Array of mechanical data Return type: list of NXOpen.Tooling.SIZERExportBuilderMechanicalData_Struct
New in version NX7.5.0.
License requirements: None.
GetRunMode¶
-
SIZERExportBuilder.
GetRunMode
¶ Gets the run mode.
Signature
GetRunMode()
Returns: Run mode Return type: NXOpen.Tooling.SIZERExportBuilderRunMode
New in version NX9.0.0.
License requirements: None.
ProcessMcdSimulationData¶
-
SIZERExportBuilder.
ProcessMcdSimulationData
¶ Processes the simulation data in MCD mode.
Signature
ProcessMcdSimulationData(startTime, endTime)
Parameters: - startTime (float) – Start Time of simulation
- endTime (float) – End Time of simulation
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetMcdMechanicalData¶
-
SIZERExportBuilder.
SetMcdMechanicalData
¶ Sets all groups of mechanical data in MCD mode.
Signature
SetMcdMechanicalData(mechanicalData)
Parameters: mechanicalData (list of NXOpen.Tooling.SIZERExportBuilderMCDMechanicalData_Struct
) – Array of mechanical dataNew in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetMechanicalData¶
-
SIZERExportBuilder.
SetMechanicalData
¶ Sets all groups of mechanical data in Motion mode.
Signature
SetMechanicalData(mechanicalData)
Parameters: mechanicalData (list of NXOpen.Tooling.SIZERExportBuilderMechanicalData_Struct
) – Array of mechanical dataNew in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
SetRunMode¶
-
SIZERExportBuilder.
SetRunMode
¶ Sets the run mode.
Signature
SetRunMode(runMode)
Parameters: runMode ( NXOpen.Tooling.SIZERExportBuilderRunMode
) – Run modeNew in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”) OR nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
SIZERExportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.