RunSimulationBuilder Class¶
-
class
NXOpen.Tooling.
RunSimulationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.RunSimulationBuilder
to animate the model, analyze the collision and reference.None is returned To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateRunSimulationBuilder()
Default values.
Property Value AngleExpression.Value 0 CheckCollision 0 ClearanceCollision 1.0 (millimeters part), 0.04 (inches part) CollisionCheckOption MeshTriangleIntersection GotoRun 0 HighlightCollision 0 IgnoreTouching 0 IntervalDimension.Value 2 StopCheckCollision 0 TimeExpression.Value 0 (millimeters part), 0 (inches part) New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AngleExpression | Returns the angle of the cycle position |
CheckCollision | Returns or sets the check collision |
ClearanceCollision | Returns or sets the clearance value of collision or interference |
CollisionCheckOption | Returns or sets the collision check method option |
GotoRun | Returns or sets the goto run angle stores the position in the cycle |
HighlightCollision | Returns or sets the highlight collision bodies flag |
IgnoreTouching | Returns or sets the ignore touching flag |
IntervalDimension | Returns the interval value of refresh |
StopCheckCollision | Returns or sets the stop check collision if find next collision |
Tag | Returns the Tag for this object. |
TimeExpression | Returns the time in the cycle |
Methods¶
Method | Description |
---|---|
CollisionConfiguration | Modify the collision by invoking collision configuration dialog |
CollisionInformation | List collision changes information in the information window |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GotoEnd | Run goto end of the simulation |
GotoStart | Goto the start of the simulation |
Next | Next simulation result |
Play | Play simulation forwards |
PlayBackwards | Play simulation backwards |
Previous | Previous simulation result |
ResetIgnoredCollision | Reset all ignored settings of the collision |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Stop | Stop simulation |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RunSimulationBuilderCollisionCheckOptions Enumeration | Specifies the collision check method |
Property Detail¶
AngleExpression¶
-
RunSimulationBuilder.
AngleExpression
¶ Returns the angle of the cycle position
-------------------------------------
Getter Method
Signature
AngleExpression()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
CheckCollision¶
-
RunSimulationBuilder.
CheckCollision
¶ Returns or sets the check collision
-------------------------------------
Getter Method
Signature
CheckCollision()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckCollision(checkCollision)
Parameters: checkCollision (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ClearanceCollision¶
-
RunSimulationBuilder.
ClearanceCollision
¶ Returns or sets the clearance value of collision or interference
-------------------------------------
Getter Method
Signature
ClearanceCollision()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceCollision(clearanceCollision)
Parameters: clearanceCollision (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
CollisionCheckOption¶
-
RunSimulationBuilder.
CollisionCheckOption
¶ Returns or sets the collision check method option
-------------------------------------
Getter Method
Signature
CollisionCheckOption()
Returns: Return type: NXOpen.Tooling.RunSimulationBuilderCollisionCheckOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollisionCheckOption(collisionCheckMethod)
Parameters: collisionCheckMethod ( NXOpen.Tooling.RunSimulationBuilderCollisionCheckOptions
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
GotoRun¶
-
RunSimulationBuilder.
GotoRun
¶ Returns or sets the goto run angle stores the position in the cycle
-------------------------------------
Getter Method
Signature
GotoRun()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GotoRun(gotoRun)
Parameters: gotoRun (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HighlightCollision¶
-
RunSimulationBuilder.
HighlightCollision
¶ Returns or sets the highlight collision bodies flag
-------------------------------------
Getter Method
Signature
HighlightCollision()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HighlightCollision(highlightCollision)
Parameters: highlightCollision (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
IgnoreTouching¶
-
RunSimulationBuilder.
IgnoreTouching
¶ Returns or sets the ignore touching flag
-------------------------------------
Getter Method
Signature
IgnoreTouching()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IgnoreTouching(ignoreTouching)
Parameters: ignoreTouching (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
IntervalDimension¶
-
RunSimulationBuilder.
IntervalDimension
¶ Returns the interval value of refresh
-------------------------------------
Getter Method
Signature
IntervalDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
StopCheckCollision¶
-
RunSimulationBuilder.
StopCheckCollision
¶ Returns or sets the stop check collision if find next collision
-------------------------------------
Getter Method
Signature
StopCheckCollision()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StopCheckCollision(stopCheckCollision)
Parameters: stopCheckCollision (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TimeExpression¶
-
RunSimulationBuilder.
TimeExpression
¶ Returns the time in the cycle
-------------------------------------
Getter Method
Signature
TimeExpression()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
CollisionConfiguration¶
-
RunSimulationBuilder.
CollisionConfiguration
¶ Modify the collision by invoking collision configuration dialog
Signature
CollisionConfiguration()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
CollisionInformation¶
-
RunSimulationBuilder.
CollisionInformation
¶ List collision changes information in the information window
Signature
CollisionInformation()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
GotoEnd¶
-
RunSimulationBuilder.
GotoEnd
¶ Run goto end of the simulation
Signature
GotoEnd()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
GotoStart¶
-
RunSimulationBuilder.
GotoStart
¶ Goto the start of the simulation
Signature
GotoStart()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Next¶
-
RunSimulationBuilder.
Next
¶ Next simulation result
Signature
Next()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Play¶
-
RunSimulationBuilder.
Play
¶ Play simulation forwards
Signature
Play()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
PlayBackwards¶
-
RunSimulationBuilder.
PlayBackwards
¶ Play simulation backwards
Signature
PlayBackwards()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Previous¶
-
RunSimulationBuilder.
Previous
¶ Previous simulation result
Signature
Previous()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ResetIgnoredCollision¶
-
RunSimulationBuilder.
ResetIgnoredCollision
¶ Reset all ignored settings of the collision
Signature
ResetIgnoredCollision()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Stop¶
-
RunSimulationBuilder.
Stop
¶ Stop simulation
Signature
Stop()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
RunSimulationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.