RemoveHolesBuilderSelectionTypes Enumeration

NXOpen.Tooling.RemoveHolesBuilder.SelectionTypes is an alias for NXOpen.Tooling.RemoveHolesBuilderSelectionTypes

class NXOpen.Tooling.RemoveHolesBuilderSelectionTypes

Bases: object

select object types, body or face

Enum Members

Enum Member Enum Member Description
Body
select body type
Face
select face type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.