ReliefDesignBuilderMethod Enumeration

NXOpen.Tooling.ReliefDesignBuilder.Method is an alias for NXOpen.Tooling.ReliefDesignBuilderMethod

class NXOpen.Tooling.ReliefDesignBuilderMethod

Bases: object

The relief design creation method.

Enum Members

Enum Member Enum Member Description
BBox
Boundbox method
UDef
User Defined method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.