QuickQuotationBuilderInsertGroupMaterials Enumeration

NXOpen.Tooling.QuickQuotationBuilder.InsertGroupMaterials is an alias for NXOpen.Tooling.QuickQuotationBuilderInsertGroupMaterials

class NXOpen.Tooling.QuickQuotationBuilderInsertGroupMaterials

Bases: object

Specify the insert group material.

Enum Members

Enum Member Enum Member Description
Cr12 insert group material is Cr12
Cr12MoV insert group material is Cr12MoV
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.