PocketBuilderToolType Enumeration

NXOpen.Tooling.PocketBuilder.ToolType is an alias for NXOpen.Tooling.PocketBuilderToolType

class NXOpen.Tooling.PocketBuilderToolType

Bases: object

Represents the select type of tool

Enum Members

Enum Member Enum Member Description
Part
part
Solid
solid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.