PiercingInsertMiniToolsBuilder Class¶
-
class
NXOpen.Tooling.
PiercingInsertMiniToolsBuilder
¶ Bases:
NXOpen.Builder
Represents piercing insert mini tools builder.
To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreatePiercingInsertMiniToolsBuilder()
Default values.
Property Value AssociationTool AddintoList New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AssociationTool | Returns or sets the association tool type. |
InsertsToDelete | Returns the inserts to delete. |
SelectAssociationInsert | Returns the selection of the inserts to create association. |
SelectAssociationScrap | Returns the selection of the scrap to create association. |
SelectScrapOrInsert | Returns the select scrap or insert for association update. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeletePiercingInsert | Delete piercing inserts which are selected. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdatePosition | Update piercing inserts position when clicking the update piercing inserts button |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PiercingInsertMiniToolsBuilderAssociationToolItems Enumeration | Specifies the association tool operation option. |
Property Detail¶
AssociationTool¶
-
PiercingInsertMiniToolsBuilder.
AssociationTool
¶ Returns or sets the association tool type.
-------------------------------------
Getter Method
Signature
AssociationTool()
Returns: Return type: NXOpen.Tooling.PiercingInsertMiniToolsBuilderAssociationToolItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssociationTool(associationTool)
Parameters: associationTool ( NXOpen.Tooling.PiercingInsertMiniToolsBuilderAssociationToolItems
) –New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
InsertsToDelete¶
-
PiercingInsertMiniToolsBuilder.
InsertsToDelete
¶ Returns the inserts to delete.
-------------------------------------
Getter Method
Signature
InsertsToDelete()
Returns: Return type: NXOpen.SelectBodyList
New in version NX11.0.0.
License requirements: None.
SelectAssociationInsert¶
-
PiercingInsertMiniToolsBuilder.
SelectAssociationInsert
¶ Returns the selection of the inserts to create association.
-------------------------------------
Getter Method
Signature
SelectAssociationInsert()
Returns: Return type: NXOpen.SelectBodyList
New in version NX11.0.0.
License requirements: None.
SelectAssociationScrap¶
-
PiercingInsertMiniToolsBuilder.
SelectAssociationScrap
¶ Returns the selection of the scrap to create association.
-------------------------------------
Getter Method
Signature
SelectAssociationScrap()
Returns: Return type: NXOpen.SelectBodyList
New in version NX11.0.0.
License requirements: None.
SelectScrapOrInsert¶
-
PiercingInsertMiniToolsBuilder.
SelectScrapOrInsert
¶ Returns the select scrap or insert for association update.
-------------------------------------
Getter Method
Signature
SelectScrapOrInsert()
Returns: Return type: NXOpen.SelectFaceList
New in version NX11.0.0.
License requirements: None.
Method Detail¶
DeletePiercingInsert¶
-
PiercingInsertMiniToolsBuilder.
DeletePiercingInsert
¶ Delete piercing inserts which are selected.
Signature
DeletePiercingInsert()
New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
UpdatePosition¶
-
PiercingInsertMiniToolsBuilder.
UpdatePosition
¶ Update piercing inserts position when clicking the update piercing inserts button
Signature
UpdatePosition()
New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
PiercingInsertMiniToolsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.