PiercingInsertBuilderTypes Enumeration

NXOpen.Tooling.PiercingInsertBuilder.Types is an alias for NXOpen.Tooling.PiercingInsertBuilderTypes

class NXOpen.Tooling.PiercingInsertBuilderTypes

Bases: object

Specifies the option of piercing insert type.

Enum Members

Enum Member Enum Member Description
DieInsert
the die insert type
DieCavityAndSlugHole
the die cavity and slug hole type
PunchInsert
the punch insert type
Association
the association type
Delete
the delete insert type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.