PiercingInsertBuilderPunchPocketTypeItemsPP Enumeration

NXOpen.Tooling.PiercingInsertBuilder.PunchPocketTypeItemsPP is an alias for NXOpen.Tooling.PiercingInsertBuilderPunchPocketTypeItemsPP

class NXOpen.Tooling.PiercingInsertBuilderPunchPocketTypeItemsPP

Bases: object

Specifies the punch pocket type in punch plate.

Enum Members

Enum Member Enum Member Description
Clearance
Punch pocket type in punch plate is clearance
Fillet
Punch pocket type in punch plate is fillet
Circle
Punch pocket type in punch plate is circle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.