PiercingInsertBuilderPunchPocketTypeItemsBP Enumeration

NXOpen.Tooling.PiercingInsertBuilder.PunchPocketTypeItemsBP is an alias for NXOpen.Tooling.PiercingInsertBuilderPunchPocketTypeItemsBP

class NXOpen.Tooling.PiercingInsertBuilderPunchPocketTypeItemsBP

Bases: object

Specifies the punch pocket type in backing plate.

Enum Members

Enum Member Enum Member Description
Clearance
Punch pocket type in backing plate is clearance
Fillet
Punch pocket type in backing plate is fillet
Circle
Punch pocket type in backing plate is circle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.