PiercingInsertBuilderNormalUdpparentPartType Enumeration

NXOpen.Tooling.PiercingInsertBuilder.NormalUdpparentPartType is an alias for NXOpen.Tooling.PiercingInsertBuilderNormalUdpparentPartType

class NXOpen.Tooling.PiercingInsertBuilderNormalUdpparentPartType

Bases: object

Specifies the parent part of user defined punch.

Enum Members

Enum Member Enum Member Description
PrjDie099
Parent part is die
PrjDb000
Parent part is db
PrjSub002
Parent part is sub
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.