PiercingInsertBuilderNormalCavityType Enumeration¶
NXOpen.Tooling.PiercingInsertBuilder.NormalCavityType is an alias for NXOpen.Tooling.PiercingInsertBuilderNormalCavityType
-
class
NXOpen.Tooling.
PiercingInsertBuilderNormalCavityType
¶ Bases:
object
Specifies the type of cavity.
Enum Members
Enum Member Enum Member Description TaperAngle the taper angle typeStep the step typeRoundStep1 the round step1 typeRoundStep2 the round step2 type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-