PiercingInsertBuilderInsertPosition Enumeration

NXOpen.Tooling.PiercingInsertBuilder.InsertPosition is an alias for NXOpen.Tooling.PiercingInsertBuilderInsertPosition

class NXOpen.Tooling.PiercingInsertBuilderInsertPosition

Bases: object

Specifies the position of piercing inserts, for EDW only

Enum Members

Enum Member Enum Member Description
Top
The position is top side
Bottom
The position is bottom side
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.