MotionSimulationBuilderTypes Enumeration

NXOpen.Tooling.MotionSimulationBuilder.Types is an alias for NXOpen.Tooling.MotionSimulationBuilderTypes

class NXOpen.Tooling.MotionSimulationBuilderTypes

Bases: object

Specifies the operation options of motion simulation.

Enum Members

Enum Member Enum Member Description
AddKinematicModel
Adds kinematic model
MountComponent
Mounts die components to kinematic components
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.