MotionSimulationBuilderMoldbaseStyleType Enumeration¶
NXOpen.Tooling.MotionSimulationBuilder.MoldbaseStyleType is an alias for NXOpen.Tooling.MotionSimulationBuilderMoldbaseStyleType
-
class
NXOpen.Tooling.
MotionSimulationBuilderMoldbaseStyleType
¶ Bases:
object
Specifies the style type of moldbase, two-plate style or three-plate style
Enum Members
Enum Member Enum Member Description Two Specifies two-plate style moldbaseThree Specifies three-plate style moldbase-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-