MotionSimulationBuilderEjectorMoveOptions Enumeration

NXOpen.Tooling.MotionSimulationBuilder.EjectorMoveOptions is an alias for NXOpen.Tooling.MotionSimulationBuilderEjectorMoveOptions

class NXOpen.Tooling.MotionSimulationBuilderEjectorMoveOptions

Bases: object

Specifies the ejector move type, after or while

Enum Members

Enum Member Enum Member Description
After
Eject product after mold fully opened
While
Eject product while mold opening
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.