ManufacturingGeometryBuilder Class¶
-
class
NXOpen.Tooling.
ManufacturingGeometryBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to be used to create manufacturing geometry.
To create a new instance of this class, use
NXOpen.Tooling.ManufacturingGeometryCollection.CreateBuilder()
Default values.
Property Value Translucency 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Face | Returns the face to use as the region faces of the geometry groups. |
Tag | Returns the Tag for this object. |
Translucency | Returns or sets the translucency to specify the group faces display. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateNewSubNode | Create a new sub node. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFaceColor | Returns the face color. |
GetObject | Returns the object currently being edited by this builder. |
InitializeContent | Sets the initialize content. |
InitializeGeometry | Sets the initialize geometry. |
SetFaceColor | Sets the face color. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Face¶
-
ManufacturingGeometryBuilder.
Face
¶ Returns the face to use as the region faces of the geometry groups.
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Translucency¶
-
ManufacturingGeometryBuilder.
Translucency
¶ Returns or sets the translucency to specify the group faces display.
-------------------------------------
Getter Method
Signature
Translucency()
Returns: Return type: int New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
-------------------------------------
Setter Method
Signature
Translucency(translucency)
Parameters: translucency (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Method Detail¶
CreateNewSubNode¶
-
ManufacturingGeometryBuilder.
CreateNewSubNode
¶ Create a new sub node.
Signature
CreateNewSubNode(selNode)
Parameters: selNode (int) – The tree new created sub node New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
GetFaceColor¶
-
ManufacturingGeometryBuilder.
GetFaceColor
¶ Returns the face color.
Signature
GetFaceColor()
Returns: Return type: int New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
InitializeContent¶
-
ManufacturingGeometryBuilder.
InitializeContent
¶ Sets the initialize content.
Parameter initialize_way indicate the different invoke entry initialize_way == 0 : Run from Electrode Design Wizard initialize_way == 1 : Run from Progressive Die Wizard initialize_way == 2 : Run from Mold Wizard initialize_way == 3 : Run from Die Design initialize_way == 4 : Run from Engineering Die Wizard.
Signature
InitializeContent(initializeWay)
Parameters: initializeWay (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
InitializeGeometry¶
-
ManufacturingGeometryBuilder.
InitializeGeometry
¶ Sets the initialize geometry.
Signature
InitializeGeometry()
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
SetFaceColor¶
-
ManufacturingGeometryBuilder.
SetFaceColor
¶ Sets the face color.
Signature
SetFaceColor(faceColor)
Parameters: faceColor (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR die_engineering (“DIE ENGINEERING”) OR ug_die_design (“Die Design”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Validate¶
-
ManufacturingGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.