MWPartingManagerBuilderRegisterType Enumeration

NXOpen.Tooling.MWPartingManagerBuilder.RegisterType is an alias for NXOpen.Tooling.MWPartingManagerBuilderRegisterType

class NXOpen.Tooling.MWPartingManagerBuilderRegisterType

Bases: object

The type of registering UNDO identifier.

Enum Members

Enum Member Enum Member Description
Init
Initialize registration for UNDO identifiers.
Current
Register current UNDO mark.
Clear
Clear all registered UNDO identifiers.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.