MWPartingManagerBuilderDataStatus Enumeration

NXOpen.Tooling.MWPartingManagerBuilder.DataStatus is an alias for NXOpen.Tooling.MWPartingManagerBuilderDataStatus

class NXOpen.Tooling.MWPartingManagerBuilderDataStatus

Bases: object

The status of the parting manager data.

Enum Members

Enum Member Enum Member Description
NotFreed
Data not freed yet.
Freed
Data already freed.
ForceUpdate
Data needs force update.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.