MWMoldedPartValidationBuilderCalculateOption Enumeration

NXOpen.Tooling.MWMoldedPartValidationBuilder.CalculateOption is an alias for NXOpen.Tooling.MWMoldedPartValidationBuilderCalculateOption

class NXOpen.Tooling.MWMoldedPartValidationBuilderCalculateOption

Bases: object

Calculation options

Enum Members

Enum Member Enum Member Description
KeepExisting
calculate and keep existing properties on the faces
EditRegionsOnly
edit properties of region faces only
ResetAll
calculate and replace all properties for region faces
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.