MWMoldedPartValidationBuilderAssignToRegion Enumeration

NXOpen.Tooling.MWMoldedPartValidationBuilder.AssignToRegion is an alias for NXOpen.Tooling.MWMoldedPartValidationBuilderAssignToRegion

class NXOpen.Tooling.MWMoldedPartValidationBuilderAssignToRegion

Bases: object

Options for assigning faces to the Cavity or Core region

Enum Members

Enum Member Enum Member Description
CavityRegion
assign selected region faces to the Cavity region
CoreRegion
assign selected region faces to the Core region
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.