MWDesignPartingSurfaceBuilderTransitionSurfaceType Enumeration

NXOpen.Tooling.MWDesignPartingSurfaceBuilder.TransitionSurfaceType is an alias for NXOpen.Tooling.MWDesignPartingSurfaceBuilderTransitionSurfaceType

class NXOpen.Tooling.MWDesignPartingSurfaceBuilderTransitionSurfaceType

Bases: object

The type of transition surface to be created.

Enum Members

Enum Member Enum Member Description
Auto
Auto transition surface
BoundedPlane
Bounded transition surface
Swept
Swept transition surface
Bridge
Bridge transition surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.