MWDesignPartingSurfaceBuilderPartingSurfaceType Enumeration

NXOpen.Tooling.MWDesignPartingSurfaceBuilder.PartingSurfaceType is an alias for NXOpen.Tooling.MWDesignPartingSurfaceBuilderPartingSurfaceType

class NXOpen.Tooling.MWDesignPartingSurfaceBuilderPartingSurfaceType

Bases: object

The type of parting surface to be created.

Enum Members

Enum Member Enum Member Description
Extrude
Extrude
Swept
Swept
BoundedPlane
Bounded plane
EnlargedSurface
Enlarge
TrimandExtend
Trim and extend
RibbonSurface
Ribbon
GuidedExtension
Guided Extension
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.