MWDesignGuideLinesBuilderDirectionType Enumeration¶
NXOpen.Tooling.MWDesignGuideLinesBuilder.DirectionType is an alias for NXOpen.Tooling.MWDesignGuideLinesBuilderDirectionType
-
class
NXOpen.Tooling.
MWDesignGuideLinesBuilderDirectionType
¶ Bases:
object
The type of direction for the guide line to be created.
Enum Members
Enum Member Enum Member Description Normal NormalTangential TangentialSnaptoWCSAxis Snap to WCS axisVector Specify Vector-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-